Other Parts Discussed in Thread: OMAPL138
Deal All:
My OMAPL138 is linked with a PHY switch(Micrel KSZ8863, it has tow PHYs), NDK is "ndk_2_20_06_35" and NSP is "nsp_1_10_00_03",and I do not modify them,and it run on OMAPL138's ARM9.The network can be up and running, but it is easy to packet loss,and I want to know wether I need to modify the NDK or NSP, and how to modify?