This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to protect condensation?



Hi all,

I use 6678 but i found if have Temperature different between board and air.It will occurecondensation. And the water can break my broard.

So, How to protect condensation? If around cover to isolate air,Can protect it?

  • Xiang_li,

    This is really an chassis/casing/environmental concern to keep moisture out.  I'm not sure you'll find the help you need on this forum.

    That said, the device is going to be operating at temps above the environmental temps since it is consuming power.  Condensation while operating should not be a concern, but it would be a potential concern when the board is in a powered down state.  I'm not sure how this is handled, but I'd assume it's an industry wide concern and that there are many ways to handle this within ones' chassis/case.

    Best Regards,

    Chad