Non riesco ad aprire i 3 file .DSN degli schematici forniti da TI (Orcad Capture 16.2).
Con Quale versione sono stati fatti?
Qualcuno è in grado di convertirli per la versione 16.2?
grazie Max
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Non riesco ad aprire i 3 file .DSN degli schematici forniti da TI (Orcad Capture 16.2).
Con Quale versione sono stati fatti?
Qualcuno è in grado di convertirli per la versione 16.2?
grazie Max
I ran this through a translator
"I can not open the file 3. DSN of the schematic provided by TI (Orcad Capture 16.2).
With Which version has been made?
Someone is able to convert them to the version 16.2?
thanks Max"
Max,
The C6657 EVM schematics are owned by eInfochips http://einfochips.com/texas-instruments/texas-instruments-tms320c6657-lite-evm-support.php
You will need to contact eInfochips for support on their Orcad files.
Here's an e-mail link for support evm6657support@einfochips.com
The AM335x is not supported in the C66x Multicore DSP Forum Section, but I'd assume it's also manufactured by a 3rd party and support of the Schematic files would be supported through that 3rd party.
Best Regards,
Chad