This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

jpeg Resizing....

Hi,

This happens on both DM355 and DM365. I have succesfully captured a UYVY image. I then Smooth it (de-interlace), and encode to jpegenc (via DMAI API). I have written some code and ported the cups library to then print that jpeg image on an IPP (CUPS) supported printer. The image is problem, but there is one problem.

The physical size of the image is HUGE - and it wants to be printed on multiple pages...etc.

Is there any type of manipulation to change the physical size of the image in order to be printed at something like the right size?

Thanks in advance

Tom