Hello,
I have problem following the "led_play" example
My problem is at step-4 (quoted below)
- Select Project->Properties, it should open Properties window for led_play project, select C/C++ Build from the left pane.
- Select Settings in the left pane after opening the C/C++ Build sub menu.
- In the Tool Settings tab, select Include Options, add following items in the Add dir to #include search path...
When I go to Project->Properties , there is no "C/C++ Build" in the left panel.
The tools I am using:
TMDSEVM6678LE
CCS 5.2.0.00069
MCSDK 2.01.00.03
CCS and MCSDK were re-installed a couple times (CCS first and then MCSDK), get the same result every time.
Your help is very much appreciated.
(This is my first time posting on the forum, hope I get everything right)
regards,
Wing