Other Parts Discussed in Thread: SYSBIOS
Dear support, I have a strange issue that I do not to resolve (i have reinstall several times and find myself in similar situation time after time)
I install in the following order:
ccs_setup_5.2.1.00018.exe (installing only the C600 libraries)
when I go in the preference window, it looks like that (which is good)
then, I install bios_mcsdk_02_01_00_03_setupwin32.exe for the C6670 only and without the IPC or sys bios modules because they are prior to the version installed on my PC.
I still have the following libraries:
c:\TI\bios_6_33_05_46 and c:\TI\bios_5_41_13_42 on my PC and I did not touch anything.
And I know that I need to install ti_cgt_c6000_7.4.1_setup_win32.exe because I need a newer compiler.
At the end of the installation, I open eclipse and discover new packages
However, here is how my preferences look like now:
Where XDC tools and sysbios and dsp bios have disappeared... and when I create a new project, let's say hello :
here is my problem:
I have try to point on the directory (which failed) and I have no idea what to do. It seems that eclipse got corrupted by the second installation
.
What do I do. I have tried to reinstall, with all packages... nothing helps.