Other Parts Discussed in Thread: TVP5146
Hi Dear TI support teams,
I used the camera driver in the BSP folder "C:\WINCE600\PLATFORM\EVM_XX3730\SRC\DRIVERS\CAMERA" , which is originated by TI and designed for analog camera by implementing decode chip TVP5146 's driver . I can run CameraDshowAPP_analog.exe which is located in the path"C:\WINCE600\PRIVATE\TEST\MULTIMEDIA\DIRECTX\DSHOW\CAMERA\CAMERAAPP" successul, it can display as expected. However, it could not run CaptureTest.exe demo which is located at the path "\PLATFORM\EVM_XX3730\SRC\APP\CaptureTest". The error information list as below,
CaptureTest: ERROR: - Could not select Composite input for video capture hr =0x80070057
CaptureTest: ERROR: Failed to create filters.
the print message can be find in the main.cpp, hr =SelectVideoCaptureInput(). This function is implemented as
HRESULT
SelectVideoCaptureInput()
{
HRESULT hr = S_OK;
//Set the capture input port
hr = pCameraControl -> Set((long)CameraControl_InputPort,(long),f_videoInput,1L)
return (hr);
}
Could you kindly help suggest which cause failures as above. Thank you!