Other Parts Discussed in Thread: AM3359
Hi,
We hit a problem when booting AM3359 from NOR Flash, here is the details:
We picked up the XIP-NOR Flash boot mode with SYSBOOT pin config set to 0x411A.
However, after the chip come out of reset, both GPMC_CSn0 and GPMC_CSn2 (ball V9 of the ZCZ package) are asserted, the assertion of CSn0 is expectable for boot flash access, but why GPMC_CSn2 has been asserted too? is that a bug in ROM code, or for any other special things?
Unfortunately, in our current design, the CSn2 is connected to another device and the assertion of this chip select will mess up the flash access during the boot.
Since there's no source for the ROM code, could anybody from TI can help to check the ROM code? Thanks a lot.
Regards
James.