This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6474 bootloader PLL mode?



Table 31 in SPRUEC6G says "For all bootmodes, the PLL is set to x16 mode."  This does not correspond with what I see on a silicon revision 2.1 DSP (DEVID.VARIANT=4).

If I connect an emulator to a DSP using boot mode 9 (DEVSTAT register value 0x00000022), trigger a warm reset for the DSP, and let the bootloader run for a while -- with no SRIO transactions being sent to the DSP -- I see the PLL1 registers stay in their reset values (PLLCTL.PLLEN=0, PLLM.PLLM=0, and so forth).

Is this the expected behavior?  Is the application responsible for programming the PLL, even if it wants x16 mode?