This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI EZSDK - VFPC : Maximum resolution?

Hi,

We have few queries on scaling and de-interlacing requirements in TI EZSDK 5_03_01_15.

1.  What is the maximum input and output resolutions supported by the VFPC component?

2. Our requirement is to give 1936 * 1112 resolution input to the VFPC. Is it possible? If yes which component should be used : DEIH, DEIM, SCAWB, NF?

3. In our experiments we have found that maximum input and output resolutions supported are 1920 * 1080. Is this a limitation in HDVPSS / VFPC component?

Please provide us the relevant information.

 Regards,

Vishwanath