This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can we do an EDMA operation from L138 to an 16 bit [DATA bus ] of an FPGA ...



Dear All , 

a) I want to do an EDMA of 512 bytes over an 16bit [DATA  interface ] FPGA memory of 1k.

b) I have done an EDMA over two memory , in which i give:-

     ACNT = 512

     BCNT =1 

     CCNT=1 whi all idex as ZERO. 

     I got proper 512 bytes of data in my destination buffer.But in this case both the source & destination was of 32 bit data bus.

c)  Now what i wanted to understand is , is it possible to do an direct EDMA [with the steps mentioned above ] to an 16 bit interface form OMAP L138.

     

Thank You,

Ashish Mishra

Banglore [INDIA]