This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Multi processor application



Hello. Im going to write an application that uses not only Cortex processor but DSP too. What libraries or drivers can you advice for it? I heard about dsp link technology and OpenCL libraries, but i dont have clear understanding about them.

Application should capture video stream via VIN0/VIN1, decode, make some warping and than display.

Regards.

  • Pavel,

    Which is the SoC that you are going to use? Which is the operating system on ARM that you will be using? Depending on these parameters, you can easily download the SDK, where all these libraries and drivers required for developing multi-core applications are available.