Other Parts Discussed in Thread: TMS320C6748, OMAP-L138
I'm using a TMS320C6748 with Flash connected using SPI1. I have an application that has been converted successfully to AIS format which I can load and execute over the serial link using UART Boot Host.
I have now built a version of the application for loading from SPI1 using AISGen and tried to load/flash it using sfh_OMAP-L138. The process hangs with a message 'Waiting for SFT on the OMAP-L138' What doest this mean? Is this because I'm using SPI1 and not SPI0
Is it possible to specify SPI1 instead of SPI0 when using sfh_OMAP-L138
Thanks
Mike.