We're running linux from TI's TI_Android_GingerBread_2_3_4Sources release, on an AM3517evm. This question pertains to a non-android build we do using configuration am3517_evm_defconfig.
We've disabled TI's kernel boot progress screen on the LCD display. So, during the kernel boot, the penguin displays on the LCD. But, after 10 minutes, the penguin disappears, simultaneous with a call being made to function sharp_lq_bl_update_status() in our LCD driver (panel-sharp-lq043t1dg01). By the way, this function wasn't in the original TI version of this driver, but I ported it over from a driver that had backlight support (panel-sharp-ls037v7dw01) and added the logs.
I want the penguin to remain on the display. So, I want this 10 minute timer to keep from firing, or perhaps to stretch it out to a huge number if that's easier.
Can anyone tell me where the value for this 10 minute timer is defined, or where the timer is actually set?
Thanks,
Ron