Other Parts Discussed in Thread: TMS320C6678
Hi
I've some questions about the boot NOR FLASH,
1) when we directly boot from EMIF16 NOR FLASH,the data lines should be x8 or x16 ,or both supported?
2) when we boot though IBL,the data lines of EMIF16 NOR FLASH should be x8 or x16 ,or both supported?
3) when we use x8 NOR FLASH for boot,according to SPRUGZ3A,we must connect C6678's address lines EMIF_A[22] to NOR FLASH's FLASH_A[0],EMIF_A[23] to FLASH_A[1],EMIF_A[0] to FLASH_A[2] and so on,is this correct?
4) when we use x16 NOR FLASH for boot,according to SPRUGZ3A,we must connect C6678's address lines EMIF_A[23] to NOR FLASH's A[0],EMIF_A[0] to FLASH_A[1],EMIF_A[1] to FLASH_A[2] and so on,is this correct?
Thanks very much for your answers.