This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM816x: H.264 decoder bit rate

Hi,

I wanted to know whether DM816x H.264 decoder is dependent of video bit rate parameter or not.

I have a requirement as below

1) to decode 4 1080p/ 4 1080i encoded streams at 15 Mbps. Is there any constraint/limitation to support maximum bit rate for each HD channel?

2) to decode 16 SD resolutions at 6 Mbps each. Is there any constraint/limitation to support maximum bit rate for each SD channel, for 16 simultaneous SD channels ?

Regards,
Sweta