the starterware (2.0.0.7) version of httpd.c is around 14KB, the version of httpd.c from the lwip project web site is around 71KB.
They are both in sub-folders of version 1.4.0 and, one would think that they would be identical.
Can anyone outline exactly happened when lwip 1.4.0(?) was ported into StarterWare?
Is the StarterWare port even useable as "normal" http server, or does the user have to re-port lwip to run on ARM?