This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 IBIS Files

The DM8168 appears to have two IBIS files. In one IBIS file, the component name is 'dm8168_pg1x'. In the other IBIS file, the component name is 'dm8168_pg2x'. Apart from slight differences in the order of pins for each component and some small differences in signal names, I can't find anything of significance that is different between the two files. The most important data - the pin-out and the models - in each file appear to be exactly the same. Can anyone tell me why there are two files and what do the 'pg1x' and 'pg2x' suffixes mean? Is it just a mistake there are two IBIS files?