This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5505 eZdsp USB Stick

I have a C5505 eZdsp USB Stick  and would like to 1) learn how to do developmental for it (home hobby stuff) and maybe do some development for it, but I have one MASSIVE road block right now, I can not figure out how to start the development for it under Linux (I do not have any windows or mac systems)  so do I have a paper weight or does any one know how to do development for it under Linux and what tools do/will I need.  And any documentation on how to upload any programs written for it to the device.

  • Good news, bad news depending on your view.  The system has a card edge for JTag programming ( not for the faint of heart, can really brick things fast ) and a SMD EEPROM. 

    Refrenced from http://support.spectrumdigital.com/boards/usbstk5505/revb/

    http://support.spectrumdigital.com/boards/usbstk5505/revb/files/usbstk5505_Schematics_revb.pdf

    So, depending how much information you can get on Linux JTag adapters/programming or how to ( in or out of system ) 512K-bit SPI EEPROM Flashing ( also not for the faint of heart for the same possible brick reason ) The Jtag adapter would be an option.  No clue where to start looking for the actual programming other than looking in to what is already Linux ready for de-bricking routers and associated JTag programmers.  I do have a home brew LPT ( buffered ) system and so far, the bricks I have tryed to unbrick turned out to be Cooked, not wrong firmware programming ( with one exception, but it was working ahead of the flashing so I knew it worked ).

    It's an option at least.

    Hope this points you in a direction to move it all forward,

    Eric

  • Thanks, if that is the only option that is the only option.  It just means the project for the dsp is going to take more time, as I still have to learn how to program a dsp also, and having to go around (as you put it) "not for the faint of heart" way, but if I was looking for easy I would not be a programmer, or using Slackware, so a bit of hard work is not something I am afraid of.