Other Parts Discussed in Thread: CCSTUDIO
hi ,
i have a problem in genrating the "_gen.c & _gen_bios.s62" , im developing application based on dm6437 encoder
im using the video_encdec sample code ,its building without clean if i cleaned the project it's not generating the above mentioned files
and showing following error .
[video_encdec.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -@"=C:/dvsdk_1_00_00_19/examples/Built_video_encdec/config/_gen.opt" -pdr -fr"C:/dvsdk_1_00_00_19/examples/Built_video_encdec/Debug" -i"C:/dvsdk_1_00_00_19/examples/Built_video_encdec" -i"." -i"../common" -i"C:/dvsdk_1_00_00_19/examples/Built_video_encdec/../../PSP_0_05_03/pspdrivers/inc" -i"C:/dvsdk_1_00_00_19/examples/Built_video_encdec/../../PSP_0_05_03/pspdrivers/drivers/inc" -i"C:/dvsdk_1_00_00_19/examples/Built_video_encdec/../../PSP_0_05_03/pspdrivers/soc/dm6437/dsp/inc" -i"C:/dvsdk_1_00_00_19/ndk_1_92_00_22_eval/packages/ti/ndk/inc" -i"C:/CCStudio_v3.3/boards/evmdm6437_v2/include/" -d"_DEBUG" -mv6400+ -@"Debug.lkf" "video_encdec.c"
[_gen.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -@"=C:/dvsdk_1_00_00_19/examples/Built_video_encdec/config/_gen.opt" -pdr -fr"C:/dvsdk_1_00_00_19/examples/Built_video_encdec/Debug" -i"C:/dvsdk_1_00_00_19/examples/Built_video_encdec" -i"." -i"../common" -i"C:/dvsdk_1_00_00_19/examples/Built_video_encdec/../../PSP_0_05_03/pspdrivers/inc" -i"C:/dvsdk_1_00_00_19/examples/Built_video_encdec/../../PSP_0_05_03/pspdrivers/drivers/inc" -i"C:/dvsdk_1_00_00_19/examples/Built_video_encdec/../../PSP_0_05_03/pspdrivers/soc/dm6437/dsp/inc" -i"C:/dvsdk_1_00_00_19/ndk_1_92_00_22_eval/packages/ti/ndk/inc" -i"C:/CCStudio_v3.3/boards/evmdm6437_v2/include/" -d"_DEBUG" -mv6400+ -@"../Debug.lkf" "_gen.c"
Fatal error: could not open source file "_gen.c"
1 fatal error detected in the compilation of "_gen.c".
Compilation terminated.
>> Compilation failure
[_gen_bios.s62] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -@"=C:/dvsdk_1_00_00_19/examples/Built_video_encdec/config/_gen.opt" -pdr -fr"C:/dvsdk_1_00_00_19/examples/Built_video_encdec/Debug" -i"C:/dvsdk_1_00_00_19/examples/Built_video_encdec" -i"." -i"../common" -i"C:/dvsdk_1_00_00_19/examples/Built_video_encdec/../../PSP_0_05_03/pspdrivers/inc" -i"C:/dvsdk_1_00_00_19/examples/Built_video_encdec/../../PSP_0_05_03/pspdrivers/drivers/inc" -i"C:/dvsdk_1_00_00_19/examples/Built_video_encdec/../../PSP_0_05_03/pspdrivers/soc/dm6437/dsp/inc" -i"C:/dvsdk_1_00_00_19/ndk_1_92_00_22_eval/packages/ti/ndk/inc" -i"C:/CCStudio_v3.3/boards/evmdm6437_v2/include/" -d"_DEBUG" -mv6400+ -@"../Debug.lkf" "_gen_bios.s62"
"_gen_bios.s62", ERROR! : [E1000] Cannot open source file _gen_bios.s62: No
such file or directory
>> Compilation failure
Build Complete,
2 Errors, 1 Warnings, 1 Remarks.
regards
vs