This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x GP EVM not reacting to SYSboot pins

Hi Champs,

My EVM has some issues with the SD boot mode. So I am trying to boot it up via Nand. However while trying to connect to the CCS the OnTargetConnect gel function is hanging for ever. I tried resetting the SYSBOOT pins 14:15 however no change in the below error message. Input frequency is still 25 MHz!

CortxA8: Output: **** AM335x 15x15 EVM Initialization is in progress ..........
CortxA8: Output: **** AM335x ALL PLL Config for OPP == OPP100 is in progress .........
CortxA8: Output: Input Clock Read from SYSBOOT[15:14]: 25MHz
CortxA8: Output: **** AM335x PLL Config failed!! Check SYSBOOT[15:14] for proper input freq config
CortxA8: Output: **** AM335x DDR2 EMIF and PHY configuration is in progress...
CortxA8: Output: EMIF PRCM is in progress .......

Can you please help?

Is there any other way I can flash the nand - UART?

Best Regards

Feroz