Hello,
I had already programmed evmc6678 board in Windows with CCS.)
Now I configured my evmc6678l board for linux according to the "Linux- c6x- 2. 0- GA User Guide"
I had completed all the Hardware setup for c6678l EVMs.
I did DIP Switching Settings to Boot from NAND and I successfully booted with Linux and I was able
to run "Out of box Demo for c66x - Linux Web control panel".
Now I want to start to program my multicore kit under Linux (Ubuntu 10.04 LTS) .
I have a few Questions.
Q1:What would be the DIP switch settings (I guess It should be in NAND boot mode)
Q2:Will the remaining procedure reamin same i.e:
Starting CCS and then set the target configuration
Launch the selected Configuration
Connect to the Target
Loading the GEL file
Then load the .out file for any demo.
Q3:The demos in MCSDK folder will also be remain same for linux .
with regards,
Muhammad Faisal,
University of Würzburg, Germany.