This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X GPMC interface ethernet chip example

Dear,

I would like to use over 3 ethernet connections with AM335X.

-AM335X has two MII interfaces that can be connected ethernet PHY chips.

-The Industrial Development Kit(IDK) has two additional ethernet ports at daughter board that have connected to AM335X' PRUS interface. And ethernet MAC layer cannot be implemented in case of PRUS interface.

Currently, I have design example that has only two ethernet connection.

In order to implement over 3 internet connection, I should connect ethernet controller(MAC+PHY) chip to AM335X GPMC interface, additionally.

My question is,

Is there any design example for ethernet controller chip that is connected AM335X  GPMC interface?

The design example would be very helpful for me to select ethernet chip and make hardware and software properly.

 

Thank you.

Best regards,

   Jay Park