Other Parts Discussed in Thread: OMAP-L137
Hello,
I'm looking for Ethernet - EMAC software examples for OMAP-L137 without DSP/BIOS. Are there any?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L137
Hello,
I'm looking for Ethernet - EMAC software examples for OMAP-L137 without DSP/BIOS. Are there any?
Thank you Mariana.
I found a package of NDK 2.0 for OMAP-L137, it is dedicated to CCSv3.3. Is there a newer package CCSv4 or CCSv5 for OMAP-L137 processor?
I've never used the embedded Linux. Where can I find examples and information on: Linux and Ethernet on OMAP ARM??
Please refer this link:
http://processors.wiki.ti.com/index.php/OMAP-L137_Software_Design_Guide
Topic: OS Support for OMAP-L137
-Thanks,
Balaji N
No, that is the only available NDK. There is an option in CCsv5 to import/convert a project from CCS3, you could try that.