Other Parts Discussed in Thread: AM3358, TPS61081
Hi,
I have an EVM with the AM3358 and want to disconnect the EVM LCD board and make my own pcb for connection to a new display and touchscreen (24-bit paraller RGB, white LED for backlight, interface mode for touchscreen: I2C, I do not have the touch-controller on my pcb, it is part of the display/touchscreen solution).
I am trying to establish what connections of the current EVM LCD board I should keep and what are not needed.
Can you answer the questions below please (my reference is the LCD board schematic) ?
1) Sheet 2 - VEXPD - Is this a 5V supply? I am going to generate this from a bench power supply. V5_0D will still come from the daughetrboard.
2) Sheet 2 - 'LCD_ENBKL' can you tell me the purpose of this pin and how it is used?can I use a GPIO of the AM3358 if needed?
3) Sheet 5 - Does this power control (U8) is needed? If I don't use it what are the implications?
Thanks,
Yu-Li