This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[ Urgent] Why address is getting incremented on EMIF interface side of OMAP L138



  

We are working on OMAP L138. We are trying to do an EDMA from KERNEL buffer to FPGA which is interfaced at EMIF.The FPGA is an 16bit[DATA ] interface.
The following are the behavior on which my doubts are based. :-

a) If my ACNT=32 ,BCNT is 1, CCNT=1,SRC_B_INDX=0, DEST_B_INDX=0, SRC_C_INDX=0, DEST_C_INDX=0.

ON EMIF side i am getting ONE ADDRESS VALUE on ADDRESS BUS.....ADRR=0

a) If my ACNT=33 ,BCNT is 1, CCNT=1,SRC_B_INDX=0, DEST_B_INDX=0, SRC_C_INDX=0, DEST_C_INDX=0.

ON EMIF side i am getting TWO ADDRESS VALUE on ADDRESS BUS.....ADRR=0 for 1st 32 byte & ADRR=1 for 2nd 32 Byte

c) a) If my ACNT=64 ,BCNT is 1, CCNT=1,SRC_B_INDX=0, DEST_B_INDX=0, SRC_C_INDX=0, DEST_C_INDX=0.

ON EMIF side i am getting TWO ADDRESS VALUE on ADDRESS BUS.....ADRR=0 for 1st 32 byte & ADRR=1 for 2nd 32 Byte

d) a) If my ACNT=66 ,BCNT is 1, CCNT=1,SRC_B_INDX=0, DEST_B_INDX=0, SRC_C_INDX=0, DEST_C_INDX=0.

ON EMIF side i am getting TWO ADDRESS VALUE on ADDRESS BUS.....ADRR=0 for 1st 32 byte & ADRR=1 for 2nd 32 Byte
ADRR=2 for 3rd 32 byte.

Can you please help me understand why there is change in address bus value obtained from EMIF even though i am doing an EDMA transfer of 32 / 33/64/66 in ASYNC mode .

As per my understanding i should get only 1 ADDR value even from EMIF interface as i am doing an DIRECT EDMA in ASYNC Mode.

The following is my code snip:-

ret = edma_alloc_channel(EDMA_CHANNEL_ANY , callback1 , NULL, dma_queue);
if ( ret < 0)
{
pr_info("The DMA DRIVER failed to get the channel ...\n");
return(ret);
}

dma_chan = ret ; // dma_chan now has the channel number being allocated


printk("CONFIGURING edma ...the source & destination...\n");
//----------------- Now setting the SRC & DEST addres ....
edma_set_src( dma_chan , (unsigned long) dmasrc , INCR ,W8BIT);
edma_set_dest( dma_chan , ( EMIF_CHIP5_BASE + (BRAM_ADDR) ) ,INCR,W8BIT);

edma_set_src_index(dma_chan , SRCBINDX , SRCCINDX) ;
edma_set_dest_index(dma_chan,DESTBIND

Thank You, 

Ashish