I'm a little confused with the system type for the AM1808 processor - in the past I'd been using a kernel with the 'DaVinci' designation for the 1808 as I believe they shared a similar code base
that was a while back however and I'm looking to update to the latest stable linux kernel
I have a few questions that I'm hoping someone can answer
-does the kernel for the 1808 come from kernel.org as-is? (can I use the 3.5.4 from http://www.kernel.org/, or must I get the kernel from TI?)
-is the 1808 a 'DaVinci' or an OMAP in the ARM system type options in 'menuconfig' of the kernel?
many thanks!