Erratum 2.1.5: System-Level ESD Immunity Usage Note
Is this a problem with ESD strikes on the oscillator traces, or anywhere on the board?
The recommended solution will draw 12.5mA @ 3.3V from the oscillator's output, above the limit for most CMOS outputs. A buffer would require an additional regulator, adding to the cost. Are there any other solutions?
Inderjit