This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debugging Qt application and ideas for my application

Dear All,

I'm working on a project in which a single master controls many slaves connected to it in rs485 communication. The master has got a display(either LCD+Touchscreen or a dvi-d monitor). The master also has got a usb keyboard and mouse. I have a beagleboard xm with me. So ideally, I will have serial working everytime with usb and there will be some processing with the data received from slaves. I am using Sitara SDK with ccsv5.

For the UI, I thought I will use Qt which comes as a integrated one with ccsv5. But Is it possible to debug my Qt application using JTAG(I have a XDS100v2 jtag with me)?

Also is it possible to access, usb (keyboard and mouse) with serial in Qt.?

If not kindly suggest me which can be used to accomplish my goal.

Regards and Thanks.