A couple of questions:
1. Is PAGESIZE in SDCR = 2n, n = number of column bits, regardless of data bus size?
2. Some industrial temp DDR2 SDRAM chips require 3.9us refresh instead of 7.8us. With tRAS(MAX) set to 70 (us), the mDDR_DDR2_Memory_Controller_Register_Calc_Rev4.xls spreadsheet has an overflow when calculating the T_RASMAX field in SDTIMR2: field value is 16 for a 4-bit field. Will a smaller value for tRAS(MAX), eg. 65 cause any issues?
3. Register SDCR2 has the ROWSIZE field. There is no place to enter it in the spreadsheet. Where in the Flash and Boot Utils is SDCR2 set?
Inderjit