This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GMII PLL clock source

The user guide (sprugz7b) has the ethernet clock in the PCIE_PLL_CFG1 register, but  other references and figure 9-2 in the same guide say that the clock comes from the SATA PLL. Which is correct for GMII?

Or if anyone has done this work of using the GMII1 interface before, would you mind sharing what registers/modifications were made?

Thank you in advance.

  • Hi Dennis,

    The GMII ref clock (125MHz) come from SATA. The whole path is: DEVOSC (20MHz) -> PCIe -> SATA -> GMAC switch. You can check the whole picture here:

    sprugz7b, 2.3.6 SERDES and Ethernet Clock Structure

    Also this thread is explaining how to enable the second ethernet port (port1):

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/214043/762567.aspx

    Best Regards,

    Pavel