Hey All,
Has any one gotten the DM8169 to work with 4 Micron MT41J128M16JT-125 or MT41K128M16JT-125 parts (2 parts per EMIF for 1GByte total)? We're having some erratic behavior and I'm not sure if it is an assembly issue or a timing issue caused by incorrect DDR3 configuration. I'm pretty sure the layout and board fabrication are ok (it's a long story). If you have, can you post the DDR settings from your GEL file?
To add a level of complication to the whole thing we couldn't get the standard DDR3 "J" parts so we installed DDR3L MT41K128M16JT-125 parts instead. It looks like the DDR3L parts should be completely compatible but any thoughts on that would be welcomed as well.
Any and all help/comments/suggestions are greatly appreciated!
Thanks,
Roz