This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DA830 vs DA810



Hi!

I am trying to port the pa_i14_evmda830 project for the Spectrum Digital eval board to our custom board which is populated with a DA810 instead of the DA830 (i.e. no ARM9 - DSP only chip). Alpha commands don't seems to be parsed/handled properly (I have tried all UART ports and I2C0 without any success) but the same code running on the eval board is working fine which leads me to believe that the ARM is still handling it. The documentation says to "simply" delete *_LINK.c / .h files from the pa/f/s19 directory to migrate from a DA830 to a DA810 but there is obviously more things to do! Any ideas or is there any CcSv4 project available for the DA810?

Thanks in advance for any help!

Louis