This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 VIP1 PortA and PortB issue

Hello Sir,

 

How to use VIP1 PortA and PortB in the MCFW ?

SDK Version: DVRRDK 3.0.0.0

Expansion I/O : REV C

 

message:

[m3vpss ]  84071: Assertion @ Line: 894 in links_m3vpss/capture/captureLink_drv.c: pInst->captureVipHandle != NULL : failed !!!

 

I found HDVPSS source code.

in the, vps/drivers/src/fvid2_drvMgr.c

 [m3vpss ]  FVID2_create:FVID2_create:617: GT_0trace 1 Driver create failed!!

 

I don't know why not use VIP1 portA or portB.

Dose it support VIP1 portA or PortB capturing in the DVRRDK 3.0.0.0 ?

 

  • Is your requirement to have only VIP PORT A and not both VIP PORT A & VIP PORT B ?

    Can you please provide the changes done to Capture Link Create Params in your usecase file.

  • Yes, I was trying VIP1 PortA or PortB of 8/16bits, but it wasn't okay.

     pCaptureInstPrm->vipInstId          = SYSTEM_CAPTURE_INST_VIP1_PORTA;

    So, I don't know why use VIP1 with PORTA giving me some error messages, but I am use a SYSTEM_CAPTURE_INST_VIP0_PORTA  of 8/16/24 bits, and it is okay.

     I found some pin mux of VIP1, but it was not setting other function.

     I look up a file (platforms/ti814x/src/vps_platformTI814x.c), and it is not setting DVO1 mode, so I think a support VIP1 capturing of 8/16 bits.

    Please see the attached file.

     

    /*
        Setup pinmux in for capture/display
    
        Pinmux setup is as shown below,
    
        VIP0
        - YCC 16-bit        - Always ENABLED
        - YCC 24-bit        - ENABLED
        - CLK0              - Always ENABLED
        - CLK1              - Always ENABLED
        - HD/VD/DE/FLD0     - ENABLED
        - HD/VD/DE/FLD1     - DISABLED
    
        VIP1
        - YCC 16-bit        - ENABLED
        - CLK0              - ENABLED
        - CLK1              - ENABLED
        - HD/VD/DE/FLD0     - DISABLED
        - HD/VD/DE/FLD1     - DISABLED
    
        VOUT0 (DVO2)
        - CLK               - Always ENABLED
        - HD/VD/DE/FLD      - ENABLED
        - YCC 16-bit        - Always ENABLED
        - YCC 20-bit        - ENABLED
        - RGB/YCC 24-bit    - ENABLED
        - RGB/YCC 30-bit    - ENABLED
    
        VOUT1 (DVO1)
        - CLK               - DISABLED
        - HD/VD/DE/FLD      - DISABLED
        - YCC 16-bit        - DISABLED
        - YCC 20-bit        - DISABLED
        - RGB/YCC 24-bit    - DISABLED
        - RGB/YCC 30-bit    - DISABLED
    
        I2C2
        - SDA               - ENABLED
        - SCL               - ENABLED
    
        HDMI I2C0
        - SDA               - ENABLED
        - SCL               - ENABLED
    */
    

    Please see the attached file, it is my MCFW capture layout.

        CaptureLink_CreateParams_Init(&capturePrm);
    
        capturePrm.numVipInst                       = 1;
        capturePrm.outQueParams[0].nextLink         = dupId;
    
        capturePrm.tilerEnable                      = FALSE;
        capturePrm.enableSdCrop                     = FALSE;
        capturePrm.fakeHdMode                       = TRUE;
    
        pCaptureInstPrm                     = &capturePrm.vipInst[0];
        pCaptureInstPrm->vipInstId          = SYSTEM_CAPTURE_INST_VIP1_PORTA;
        pCaptureInstPrm->videoDecoderId     = SYSTEM_DEVICE_VID_DEC_TVP7002_DRV;
        pCaptureInstPrm->inDataFormat       = SYSTEM_DF_YUV422I_YUYV;
        pCaptureInstPrm->standard           = SYSTEM_STD_1080P_60;
        pCaptureInstPrm->numOutput          = 1;
    
        pCaptureOutPrm                      = &pCaptureInstPrm->outParams[0];
        pCaptureOutPrm->dataFormat          = SYSTEM_DF_YUV422I_YUYV;
        pCaptureOutPrm->scEnable            = FALSE;
        pCaptureOutPrm->scOutWidth          = 0;
        pCaptureOutPrm->scOutHeight         = 0;
        pCaptureOutPrm->outQueId            = 0;

    Thank you very much for your support

  • Hi Badri,

    I am trying to do a 8-bit bt.656 embedded sync stream capture on VIP2 PORTB using OMX application . I am using EZSDK 5.04 .

    The OMX app is not capturing frames on VIP2 PORTB ,But I can capture bt.656 stream on VIP1 PORTA using the same OMX app . Can you comment about bt.656 capture on PORTB using OMX app?

  • Hi Yeh and Sivaramkrishna,

    Have you guys been able make the VIP1 PortB work after all?

    I'm in a similar situation right now.  
    I have a custom DM8148 board with 4 tvp5150s, connected to VIP0-PortA, VIP0-PortB, VIP1-PortA and VIP1-PortB.   I can capture video from all ports except for VIP1-PortB.  I would like to know if it is possible to capture from VIP1-PortB before spending too much time on hacking the driver.

    I use EZSDK 5_05_02_00, with modified capture driver.  Tvp5150s are configured to output BT656 format.

    Thanks,
    tamo2