Hi all:
I am developping on DM36X IPNC REF 3.0, our board has changed to USB HOST mode, and I choose "USB HOST" mode, "USB DEVICE FS", "USB MASS STORAGE" build in. Now when I plug in one USB disk. the system can detect the USB disk, prompt info is below:
********************************************************************************************************************************************
[ 943.130000] usb 1-1: new high speed USB device using musb_hdrc and address 9
[ 943.290000] usb 1-1: configuration #1 chosen from 1 choice
[ 943.370000] scsi3 : SCSI emulation for USB Mass Storage devices
[ 948.430000] Vendor: USB2.0 Model: Flash Disk Rev: 2.60
[ 948.440000] Type: Direct-Access ANSI SCSI revision: 02
[ 948.480000] SCSI device sda: 4136960 512-byte hdwr sectors (2118 MB)
[ 948.480000] sda: Write Protect is off
[ 948.490000] sda: assuming drive cache: write through
[ 948.500000] SCSI device sda: 4136960 512-byte hdwr sectors (2118 MB)
[ 948.520000] sda: Write Protect is off
[ 948.520000] sda: assuming drive cache: write through
[ 948.530000] sda:<7>usb-storage: queuecommand called
[ 948.550000] unknown partition table
[ 948.580000] sd 3:0:0:0: Attached scsi removable disk sda
[ 948.680000] sd 3:0:0:0: Attached scsi generic sg0 type 0
********************************************************************************************************************************************
but under /dev/, there is no sda* , mabe the kernel can detect USB device, but can not create dev under /dev, what is the reason about this ?
BERT REGARDS
Steven