This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to bring the UVC camera up for DM8148 Android GingerBread

Hi All,

I am working on DM8148 EVM.  Recently I have ported Android GingerBread and am able to see Android in LCD. Now I want to capture video using usb camera. So I connected USB camera to board and I opened the camera on LCD. But there is nothing coming. When I connected my camera to board, Board detecting camera and am able to see /dev/Video 0, Video 1 in devices. Do I need to load any USB camera drivers? Please  suggest some solutions regarding this issue.