Hello,
I am working with customer who used leopard board ref.design for making the wild life camera project, they used same ref.schematic,Bill of material including CMOS lense According to Leopard Ref.Design it produce images upto 5MP, but customer can only get 0.9 MP with 5MP camera interfaced with DM355 processor, they are suspecting the capability of the processor.
Below are the details of the software version details:
OS: Linux Kernel 2.6.10
SDK: DVSDK 1.30.01.41
The sensor is MT9P031 (5 MP)
Regards,
Datta