This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP4: Android ICS on Blaze (4430) ES2.2 EMU device

Other Parts Discussed in Thread: 4430

Hi all,

I have downloaded the prebuilt boot images from omappedia.

I tried to boot it, but it is rebooting after "Uncompressing linux...." message.

Texas Instruments Inc X-Loader 1.41.0-g28b5a696 (Jul 25 2012 - 08:47:55)
mmc read: Invalid size
Starting OS Bootloader from MMC/SD1 ...


U-Boot 1.1.4-g83ec135f (Sep 24 2012 - 16:30:48)

Load address: 0x80e80000
DRAM: 1024 MB
Flash: 0 kB
Using default environment

In: serial
Out: serial
Err: serial
Initializing SD(0) Slot.
ptbl slot: SD:(0).
efi partition table not found
efi partition table:
ptbl slot: EMMC:(1).
256 128K xloader
512 2M bootloader
4608 128K misc
4864 384K env
5632 8M recovery
22016 8M boot
38400 512M system
1086976 256M cache
1611264 512M userdata
2659840 8M boot1
2676224 512M system1
3724800 256M cache1
4249088 512M userdata1
5297664 4989M media
Net: KS8851SNL
Hit any key to stop autoboot: 0
OMAP44XX SDP #
OMAP44XX SDP # setenv bootargs console=ttyO2,115200n8 mem=1G androidboot.console=ttyO2 mem=512M root=/dev/mmcblk1p2 rw rootdelay=2 init=/init vram="32M" omapfb
.vram="0:16M,1:16M" vmalloc=768M omap_wdt.timer_margin=30
OMAP44XX SDP # setenv bootcmd 'mmcinit 0; fatload mmc 0 0x80000000 uImage;bootm 80000000'
OMAP44XX SDP # run bootcmd
mmc read: Invalid size

4449748 bytes read
## Booting image at 80000000 ...
Image Name: Linux-3.0.31-01830-g89e862c
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4449684 Bytes = 4.2 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
OK
I2C read: I/O error

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

PPA supports 4430 > ES2.1 only
Detected device: 04430e22 EMU
PPA 1.8.3 hash fd31d754, ONLY PUBLIC DEBUG ON
!OBFUSCATOR ON!
SEC_STATUS = 0003fba2
Free space for PPA: 3092 bytes
The PPA is about to free 2544 bytes

Any inputs?

Regards,

Ramya.M