Other Parts Discussed in Thread: SYSBIOS
Hi,
" I am using Version: 5.2.1.00018. When i try to make a new project with SYSBIOS (standart hello example), When i tried to build, it gives me this error. When i looked into std.h with Right click-> Open declaration file everything seems ok. I was using Code Composer v4 before and it still loaded in my computer. Problem can be related with this? I've tried the solve the problem for 3 hours. Thanks for help. "
That was my first problem and I have added c/c++ General / Paths and Symbols/ Includes directory of xdctools , BIOS and ccs_base and now it gives another errors not xdc/std.h missing. Copy and paste from CDT Build Console :
**** Build of configuration Debug for project SYS 1 ****
C:\ti\ccsv5\utils\bin\gmake -k all
'Building file: ../app.cfg'
'Invoking: XDCtools'
"C:/ti/xdctools_3_23_03_53/xs" --xdcpath="C:/ti/bios_6_33_05_46/packages;C:/ti/ccsv5/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M3 -p ti.platforms.stellaris:LM3S9D96 -r release -c "C:/ti/ccsv5/tools/compiler/tms470_4.9.5" --compileOptions "-g --optimize_with_debug"
Usage: xs xdc.tools.configuro [--help]
[-v | -q]
[-@ optionsfile]
[-o outdir]
[-b config_bld | -c codegen_dir | --cb]
[-t target] [-p platform[:instance]] [-r profile]
[-Dname=value]
[-w | -x regexp]
[--rtsName pkg_name]
[--cfgArgs args_string]
[--linkTemplate linker_template]
[--tcf] [--bios5] [--pkg] [--generationOnly]
[--compileOptions compile_options_string]
[--oc compiler.opt] [--ol linker.cmd]
infile.cfg
'Finished building: ../app.cfg'
' '
'Building file: ../main.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv5/tools/compiler/tms470_4.9.5/bin/cl470" -mv7M3 --code_state=16 --abi=eabi -me -g --include_path="C:/ti/ccsv5/tools/compiler/tms470_4.9.5/include" --include_path="C:/ti/xdctools_3_23_03_53/packages" --include_path="C:/ti/bios_6_33_05_46/packages" --include_path="C:/ti/ccsv5/ccs_base" --diag_warning=225 --display_error_number --preproc_with_compile --preproc_dependency="main.pp" --cmd_file="./configPkg/compiler.opt" "../main.c"
>> ERROR: Cannot open command file './configPkg/compiler.opt': No such file or directory
'Finished building: ../main.c'
' '
'Building target: SYS 1.out'
'Invoking: ARM Linker'
"C:/ti/ccsv5/tools/compiler/tms470_4.9.5/bin/cl470" -mv7M3 --code_state=16 --abi=eabi -me -g --diag_warning=225 --display_error_number -z --stack_size=256 -m"SYS 1.map" --heap_size=0 -i"C:/ti/ccsv5/tools/compiler/tms470_4.9.5/lib" -i"C:/ti/ccsv5/tools/compiler/tms470_4.9.5/include" --reread_libs --warn_sections --display_error_number --rom_model -o "SYS 1.out" -l"./configPkg/linker.cmd" "./main.obj" -l"libc.a" "../lm3s9d96.cmd"
<Linking>
error #10008-D: cannot find file "./configPkg/linker.cmd"
>> Compilation failure
undefined first referenced
symbol in file
--------- ----------------
ti_sysbios_BIOS_start__E ./main.obj
ti_sysbios_knl_Task_sleep__E ./main.obj
xdc_runtime_System_printf__E ./main.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "SYS 1.out" not built
gmake: *** [SYS 1.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
------------------------------------------------------------------------------
Errors are :
Description Resource Path Location Type #10008-D cannot find file "./configPkg/linker.cmd" SYS 1 C/C++ Problem
Description Resource Path Location Type #10010 errors encountered during linking; "SYS 1.out" not built SYS 1 C/C++ Problem
Description Resource Path Location Type <a href="file:/C:/ti/ccsv5/tools/compiler/dmed/HTML/10234.html">#10234-D</a> unresolved symbols remain SYS 1 C/C++ Problem
Description Resource Path Location Type Unresolved symbol ti_sysbios_BIOS_start__E in file ./main.obj .xdchelp /SYS 1 0 C/C++ Problem
Description Resource Path Location Type Unresolved symbol ti_sysbios_knl_Task_sleep__E in file ./main.obj .xdchelp /SYS 1 0 C/C++ Problem
Description Resource Path Location Type Unresolved symbol xdc_runtime_System_printf__E in file ./main.obj .xdchelp /SYS 1 0 C/C++ Problem
What is the Problem? it seems Linker problem but i couldn't solve it. Thanks for help.