This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code Generation from a MATLAB-m-function - C6748 Teaching Materials - NOT WORKING!!!



Hello,

the Exsample "Code Generation from a MATLAB m-function" from the C6748 Teaching Rom ist not working at all. I Used CCSv4 and Matlab Release 2011b, as you suggested there. But there are just 1000 of errors at the build.

Here are the errors:
I did exactly the way described in the teaching materials! Why are these exsamples false? I need information about that PLEASE!

Has anyone tested it successfully?

Greatings, Janek Rathjen.


ERRORS:


**** Build of configuration Debug for project matlab_test_algo ****

C:\Program Files\Texas Instruments\ccsv4\utils\gmake\gmake -k all
'Building file: ../main.c'
'Invoking: Compiler'
"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c6000/bin/cl6x" -mv6740 -g --include_path="C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c6000/include" --include_path="C:/Program Files/MATLAB/R2011a/extern/include" --include_path="C:/Program Files/MATLAB/R2011a/simulink/include" --diag_warning=225 --abi=coffabi --preproc_with_compile --preproc_dependency="main.pp"  "../main.c"
"C:/Program Files/MATLAB/R2011a/extern/include/emlrt.h", line 473: warning: type qualifier on return type is meaningless
"../main.c", line 9: warning: last line of file ends without a newline
'Finished building: ../main.c'
' '
'Building target: matlab_test_algo.out'
'Invoking: Linker'
"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c6000/bin/cl6x" -mv6740 -g --diag_warning=225 --abi=coffabi -z -m"matlab_test_algo.map" --warn_sections -i"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c6000/lib" -i"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c6000/include" --reread_libs --rom_model -o "matlab_test_algo.out"  "./norm.obj" "./my_inverse_terminate.obj" "./my_inverse_mex.obj" "./my_inverse_initialize.obj" "./my_inverse_api.obj" "./my_inverse.obj" "./main.obj" -l"rts6740.lib"
<Linking>
warning: creating ".stack" section with default size of 0x400; use the -stack
  option to change the default size

undefined                first referenced    
 symbol                      in file         
---------                ----------------    
_emlrtAlias              ./my_inverse_api.obj
_emlrtAssign             ./my_inverse_api.obj
_emlrtCallMATLAB         ./my_inverse.obj    
_emlrtCheckBuiltInR2011a ./my_inverse_api.obj
_emlrtDestroyArray       ./my_inverse_api.obj
_emlrtImportCharArray    ./my_inverse.obj    
_emlrtInitCharArray      ./my_inverse.obj    
_emlrtPopRtStack         ./norm.obj          
_emlrtPushRtStack        ./norm.obj          
_muDoubleScalarAbs       ./norm.obj          
_muDoubleScalarIsNaN     ./norm.obj          
_mxCreateCharArray_730   ./my_inverse.obj    
_mxCreateDoubleScalar    ./my_inverse.obj    
_mxGetNaN                ./norm.obj          

error: unresolved symbols remain
error: errors encountered during linking; "matlab_test_algo.out" not built

>> Compilation failure
gmake: *** [matlab_test_algo.out] Error 1
gmake: Target `all' not remade because of errors.
Build complete for project matlab_test_algo

  • Janek,

    Since no one replied all day, I will at least offer a comment. I am not directly familiar with the examples you are referencing and have not used them or Matlab.

    Your linker errors mean that there is a library (or more than one library) that is missing. There is no Matlab library named in your linker commands list, so there must be one or more required for your example. Please check closely and follow the directions supplied exactly. Do not try to build your own project or try to do things a little differently. All installations must be done as stated from the beginning of the process.

    Regards,
    RandyP