hi,
We are using TMS320DA828 custom board. PSP version is 2.00.01 which was originally meant for DSKDA830EVM.
According to the datasheets i2c0 should get the clock from Auxclock. Since DSKDA830EVEM's crystal is 24Mhz, auxclk should also be 24Mhz.But in packages\ti\psp\cslr\soc.xs file the i2c0 inputFrequency is mentioned as 50000000Hz(50Mhz) which is in contradiction to the datasheet(?). In our custom da828 board we have 24Mhz crystal.So I am confused whether I should give 24Mhz as the inputFrequency or should it be 50Mhz? Can somebody please help us on this?
Thanks and Regards,
Rajaram