Hi all,
I have the following situation, where the same program works and alternatively doesn't.
When I download the .out file through the debugger the software runs as desired.
When I create an Ethernet download image, I download it, then in the debugger set the PC to the _c_int00 of the program and run it, the program gets lost running functions that look like TI_zero_init and TI_decompress_rle.
Does the choice of abi change the way the ethernet image is generated? Which step should be affected: hex6x, mergebtbl, bcovert64x or bootpacket?
Do you have any suggestions?
Regards,
e