Other Parts Discussed in Thread: OMAPL138
I use OMAPL138, I use DSP only, I have got OMAPL138_StarterWare_1_10_03_03, now I have porblem in use nandflash.
the code as follow:
retVal = NANDBlockErase(&nandInfo, blkNum);
this is from nandflash lib, but it return 9, I donot kwow what it mean.
the return values in nandlib.h as follow:
typedef enum _NAND_STATUS_
{
NAND_STATUS_PASSED = (0x001),
NAND_STATUS_FAILED = (0x002),
NAND_STATUS_NOT_FOUND = (0x004),
NAND_STATUS_DEVBUSY = (0x008),
NAND_STATUS_DEVWRPROTECT = (0x010),
NAND_STATUS_WAITTIMEOUT = (0x020),
NAND_STATUS_READWRITE_DMA_FAIL = (0x040),
NAND_STATUS_ECC_UNSUPPORTED = (0x080),
NAND_STATUS_READ_ECC_ERROR_CORRECTED = (0x100),
NAND_STATUS_READ_ECC_UNCORRECTABLE_ERROR = (0x200)
}
NandStatus_t;
the nandflash I used is K9F4G08U0B.
Why?