Other Parts Discussed in Thread: DM385
Hi,
We are looking at the possibilities of encoding HDR video using an omap4460, and would like to know about possible limitations before we dive to deep into this subject.
Our sensor candidate can be set to use alternate row timings for HDR. (odd lines will have a different exposure time then even lines, and merging information from both lines could give HDR video, either at an increased bit depth, or after a process called tone mapping using “normal” bit depths.
1) Is this an application that TI have ever considered?
2) Does there exist any ducati codecs encoding at higher bit-depths then normal?
3) Would we really have to do the tone mapping in the main CPU? (Is there any way we could use the ISP? Is the hardware even able to look at non-adjacent lines and do more than simple filtering operations?)
4) Would there be some other way of encoding HDR video that we aren’t aware of, or a different product. (and btw, the provided dynamic range extension is not an option for us)
As far as possible, we would like to avoid having to use either the CPU or an external FPGA to do the video processing.
BR
/Simon