Other Parts Discussed in Thread: TMS320C6678
I'm a beginner and I'm trying to follow the quick start guide.
In step 4 I receive by the hyper Terminal the following message:
IBL: PLL and DDR Initialization Complete
IBL Result code 00
IBL: Booting from NOR
Start BIOS 6
QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
HUA version 2.00.00.04
Setting hostname to tidemo-063255
MAC Address: 40-5F-C2-9C-08-17
Configuring DHCP client
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Registration of the EMAC Successful, waiting for link up ..
Service Status: DHCPC : Enabled : : 000
Service Status: THTTP : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
I don't see any IP address..