Other Parts Discussed in Thread: AM3703, TUSB1210, AM3505
I have a custom AM3703 design that uses the TUSB1210 PHY on the HSUSB0 (otg/host/device) USB port. The TUSB1210 PHY is set up as the ULPI clock source and has a proper 3.3V 26MHz reference clock oscillator connected to its REFCLK pin.
I'm using a 2.6.39 Linux Kernel from a TI released SDK (modified somewhat to support my board).
In the software, I'm using the "usb_nop_xceiv" transceiver object, just like the omap3evm (which has an ISP1504 transceiver). Should I be using anything else?
Currently, I can load the "g_ether" kernel module and do a lot of pinging, but lose connections when I try to move a lot of data. dmesg prints out a whole mess of messages, more-or-less cycling among:
[ 684.263000] g_ether gadget: suspend
[ 684.692932] g_ether gadget: reset config
[ 684.692962] g_ether gadget: ecm deactivated
[ 684.692993] usb0: gether_disconnect
[ 684.859405] musb_g_ep0_irq 709: SetupEnd came in a wrong ep0stage idle
[ 684.866638] musb_g_ep0_irq 709: SetupEnd came in a wrong ep0stage setup
[ 684.873687] musb_g_ep0_irq 709: SetupEnd came in a wrong ep0stage out/status
[ 684.881103] musb_g_ep0_irq 801: SETUP packet len 0 != 8 ?
[ 684.886871] musb_g_ep0_irq 709: SetupEnd came in a wrong ep0stage out/status
[ 684.895477] g_ether gadget: high speed config #1: CDC Ethernet (ECM)
[ 684.895507] musb-hdrc periph: enabled ep2in for int IN, dma, maxpacket 16
[ 684.895538] g_ether gadget: init ecm
[ 684.895568] g_ether gadget: notify connect true
[ 684.896301] g_ether gadget: activate ecm
[ 684.896331] musb-hdrc periph: enabled ep1in for bulk IN, dma, maxpacket 512
[ 684.896362] musb-hdrc periph: enabled ep1out for bulk OUT, dma, maxpacket 512
[ 684.896392] usb0: qlen 10
[ 684.896423] g_ether gadget: ecm_open
[ 684.896453] usb0: eth_start
[ 684.896728] musb_g_ep0_irq 709: SetupEnd came in a wrong ep0stage idle
I'm wondering if I'm on the completely wrong track here. Things seem to mostly work, because I can get the g_ether device to turn on and enumerate on the host, and setup as an Ethernet device driver. I can get pings across. So what might be wrong?
Ideas:
- I need to setup the platform_data somehow to indicate that the PHY is the ULPI clock source instead of the AM3703.
- The 2.6.39 USB device code isn't stable.
- I need to use a different "otg_transceiver" object.
- No one has ever used the TUSB1210 (or similar) for the OTG/Device port (HSUSB0) on an AM3703 before and I should change my hardware.