Hi expert,
We use OMAP4460 and TWL6032 in our project.
When booting, if the system is running in u-boot, all the power supply of TWL6032 is fine.
But when linux kernel is start to run, the power supply VMMC, and REGEN1 are power down. Then linux kernel can't copy files from SD card.
I don't know what is the problem, please help me.
By the way, can anyone explain the working principles of PMIC and OMAP4 ? How does OMAP4 control the PMIC in different conditions (active,idle,sleep,wait)?
How does OMAP4460 control the Power on/off of PMIC REGEN1,REGEN2, and LDOs by I2C interface?
Best regards.