Hi ,
i am integrating mt9m112 to beagleboardxm
kernel 2.6.37 (ginger bread release)
the camera sensor signals d0 t0 d11 are connected to cam_d0 to cam_d11
getting signals for camera d2 t0 d11 from the camera sensor
the configuration in board-opam3beagle-camera.c
.subdevs = beagle_camera_primary_subdevs,
.interface = ISP_INTERFACE_PARALLEL,
.bus = {
.parallel = {
.data_lane_shift = 2,
.clk_pol = 0,
.bridge = 3,
i was able to get the test pattern but it is slightly different from expected pattern
i want to use the signals cam_d2 t0 cam_d11 only.
can any one point the correct values for data_lane_shift and bridge
to obtain correct signals to CCDC
Regards,
Dibin