Hi, all,
We are using DVRRDK-03.00.00.00 on P.G. 2.0 of DM8168, when usb overcurrent occurs, USB_DRVVBUS(Pin P35, R35) output Low Signal to disable external usb power, and then resume to normal mode ( remove overcurrnt device), USB_DRVVBUS still output Low Signal,and therefore external USB Power always disabled. Once the usb port encounters overcurrent then resume to normal mode, the usb port can't be used again unless system reboot.,
Unfortunately, everything about overcurrent on USB ports is all right in DVRRDK-02.80.00.10 on P.G. 2.0 of DM8168.
Any suggestion will be appreciated, thanks.