This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMAC in xgconf is not enabled

Hello,

I want to use my OMAPL137 as server and whenever there is a request from client (PC), server has to send some data. For this, I am using NDK 2.0. I have figured out that for OMAP L138, there exists an NSP but for other processors, it is included in development kit. In that case, I expect it to be already existing. But then in CCS 5, in xgconf, the option EMAC in data link layer is not enabled. It is also not shown in Available Products --> NDK core stack --> data link layer. The data link layer has only two options i.e. Ppp and Pppoe. But for my task I need EMAC. Also, I dont find related examples in NDK folder.

Can you please help me as it is becoming really confusing?

Please see if something is unclear, please feel free to question.

Thanks in advance.

Best Regards,

Mini Kaushik